Associate II
May 31, 2016
Question
L6470 abs_pos bit length not as large as literature claims? & busy pin ending early.
- May 31, 2016
- 2 replies
- 917 views
Posted on May 31, 2016 at 03:18
From the literature, the abs_pos value is a 22 bit 2's complement integer. but when i move the position above 32768 (16 bit 2s complement maximum), the value resets to negative. I.e. the abs_pos value acts as a 16 bit 2s complement value.
Additionally, using the dSPIN_Move command and using the dSPIN_BUSY to check to make sure it's finished with the move, the busy pin will go high early and the move will not finish. I.e. i will send a dSPIN_Move(''FWD'',4000) and it will only move so far, then stop without completing the commanded move from the abs_pos before the dSPIN_BUSY goes high. Has anyone else has these issues? Some guidance would help, besides these issues, the product works great.attached is data output from the abs_pos (see line 28774 for example of it ending early) and sample code of how i'm commanding it. #l6470