Skip to main content
Visitor
July 14, 2026
Question

L6387ED with an STM32G431

  • July 14, 2026
  • 0 replies
  • 33 views

We are considering using the L6387ED with an STM32G431 powered at 3.3 V.

The L6387ED datasheet appears to specify a minimum input high-level threshold, VIHV_{IH}VIH​, of 3.6 V under some conditions, which would not guarantee recognition of a 3.3 V STM32 GPIO high level over process, voltage and temperature.

However, the ST B-G431B-ESC1 reference board appears to connect STM32G431 3.3 V PWM outputs directly to L6387ED inputs.

Could you please confirm the following:

  1. Is direct connection of a 3.3 V STM32G431 GPIO to the L6387ED input officially guaranteed across the full operating temperature range and production tolerances?
  2. If yes, which datasheet specification or characterization data guarantees this compatibility?
  3. What is the guaranteed maximum VIHV_{IH}VIH​ for the L6387ED at VCC=12–15 VV_{CC}=12\text{–}15\ \mathrm VVCC​=12–15 V, over the full recommended temperature range?
  4. Does the B-G431B-ESC1 rely on typical rather than guaranteed input thresholds?
  5. If direct 3.3 V drive is not guaranteed, which level-shifting or buffer solution does ST recommend between the STM32G431 and the L6387ED?
  6. Are the L6387ED inputs 5 V tolerant when the device is powered, unpowered, or during power sequencing?

This clarification is required for a production design, not only for a laboratory prototype.