Skip to main content
Associate II
March 18, 2025
Question

l6235q motor speed

Hi

I have a motor contol design for a 4pole motor 4800 rpm but my control seem to be limiting the speed to 300-500rpm

I have followed the app note AN1625 and using a integrator circuit. I can adjust vspeed voltage via a pot. but this does not change the speed much.

I have set my Tpulse to 282us 

RCOFF parts are is 1nf and 33k.

my integrator is a 5v signal rail with the feedback of 1meg and a 220nf cap. A 5.6k / 1.8k resistor divider on the output. which feed Vref of the L6235.

what am i doing wrong. do i need to ajust my resistor network?

regards

Ross

 

 

 

 

This topic has been closed for replies.

1 reply

Associate II
March 24, 2025

hi

 update, hall effect filter causing the issue now running at 8500rpm with 25v or 6000 rpm at 20v. need to run 600rpm at 28v. do i need to increase my rcoff time?