Skip to main content
marek23
Visitor II
April 4, 2013
Question

L6234 Vref capacitor

Posted on April 04, 2013 at 20:26

The AN1088 app note states:

�

Vref ( Voltage Reference).

This is the internal 10V voltage reference pin to bias the logic and the low voltage circuitry of the device. A 1

m

F electrolytic capacitor connected from this pin to GND ensures the stability of the DMOS drive circuit. This pin can be externally loaded up to 5mA. Figure 3 and 4 show the typical behavior of the Vref pin.�

I was wondering whether a higher value ceramic capacitor can be used in place of the 1uF electrolytic capacitor on the Vref pin. For example, can we use a 4.7uF, 25V, ceramic, such as  C1608JB1E475K080AC? The app note does not describe whether there are other capacitor options.

Thanks!

#l6234-an1088
This topic has been closed for replies.

6 replies

Enrico Poli
ST Employee
April 10, 2013
Posted on April 10, 2013 at 17:21

The VREF capacitor can be ceramic, but its value should be >= of 1uF.

So the capacitor you indicated is OK.

Regards

Enrico

MQi.1
Senior II
May 17, 2024

I read from datasheet "10 V external reference available", while I tested 8.8v at Vref by a 12v battery source, could I added an external 10v to this pin?

AScha.3
Super User
May 17, 2024

> "10 V external reference available", while I tested 8.8v at Vref by a 12v battery

from ds:

AScha3_0-1715936135249.png

So at 12V supply about 8.8 V are exactly what it should be.

If you feel a post has answered your question, please click on " Best Answer ".