Skip to main content
sHL
Associate
January 27, 2019
Question

L6229 ic burning during programming STM32L162VE controller using JTAG.

  • January 27, 2019
  • 2 replies
  • 678 views

L6229 ic interfaced to STM32L162VE controller. L6229 ic burning during programming STM32L162VE controller using JTAG. it will be helpful if i get any hints to debug the issue

This topic has been closed for replies.

2 replies

S.Ma
Principal
January 27, 2019

Hmm, for brushless motor control there are 6 outputs from timer with 3 negated sones.

When the MCU is under reset, these GPIO are not driving the outputs, such as when reflashing the micro.

Maybe put weak pull-up/down on these lines to ensure safe operation.

sHL
sHLAuthor
Associate
January 27, 2019

Thank you

i will check and verify this point