Skip to main content
mahmoud2
Visitor II
April 13, 2016
Question

L6226Q broken when Vs pin is rapidly switched on and off ?

  • April 13, 2016
  • 0 replies
  • 487 views
Posted on April 13, 2016 at 11:48

Hello,

I am using the eval board EVAL6226QR that has the dual full bridge driver L6226Q on it.

I am using it to drive a 40kHz train of pulses from IN1A to OUT1A (and IN2A to OUT2A).

To minimize current consumption, I am controlling the Vs pin (that has 32V on it) by a window that goes HIGH for 500 microseconds, and LOW for 30 milliseconds.

After few tests (sometimes, that happens after few days of proper operation), the HBRIDGE breaks down ! (there are high current peaks detected on my voltage generator higher than 1Amp !)

This is the fifth EVAL6226QR that breaks down now !

Feeding Vs with continuous voltage does not cause the hbridge to break down (but it consumes 120mA which is too high)

I looked carefully into the datasheet of the eval board and that of the chip, and I found only frequency characteristics for IN pins only (Vs is supposed to have a constant voltage apparently)

Does it mean that it is not meant to have its Vs pin fed with AC voltage ?

Can anyone suggest a solution for this please ?

PS : I don't want to feed this window signal to ENA pin because when LOW, outputs go high impedance and not low state

#eval6226qr #h-bridge #l6226q
This topic has been closed for replies.