Skip to main content
B.Michele
Associate III
January 29, 2014
Question

L6207 signal and control With 3V3 ucontroller

  • January 29, 2014
  • 2 replies
  • 631 views
Posted on January 29, 2014 at 13:04

Hy, i must use a full bridge driver L6297 for control two normal DC motor 24V.

My uP is  STM32 Cortex STM32F100 with 3,3 Volt supply.

Can i control direcly the L6207 with 3,3 Volt level ?? for all the signal control:

In digital, enable, pwm, Vref .....

Thank you
This topic has been closed for replies.

2 replies

Enrico Poli
ST Employee
February 3, 2014
Posted on February 03, 2014 at 11:38

Hi, all the digital inputs of the L6207 are compliant with the 3.3 V logic signals and you can ajust the VREF using a 3.3 V PWM without any limitation.

Regards

Enrico

B.Michele
B.MicheleAuthor
Associate III
February 3, 2014
Posted on February 03, 2014 at 12:43

Thank you very much

Best regards

Michele