Skip to main content
k-takagi
Visitor II
August 27, 2013
Question

L6207 - Cboost connetion

  • August 27, 2013
  • 1 reply
  • 554 views
Posted on August 27, 2013 at 02:52

According to the datasheet, Cboost(220nF/100V) is connected between VBOOST pin and VS pin. But according to the EVKIT schematic, Cboost is connected between VBOOST pin and GND. Which connection is more recommended?

l6207-boost

This topic has been closed for replies.

1 reply

Enrico Poli
ST Employee
September 4, 2013
Posted on September 04, 2013 at 14:43

Hello,

the boost capacitor can be connected both to VS or ground.

Connecting the capacitor to VS is the suggested solution because it allows to use a lower voltage rating capacitor.

Regards

Enrico