Skip to main content
Pawe? Flisikowski
Associate
October 20, 2017
Question

L5973D step down regulator

Posted on October 20, 2017 at 14:16

Hi,

I'm repairing an audio power amplifiers from a top model manufacturer like Harman-Kardon, Dynaudio, Bose from cars. And in almost all of models I faceing up with broken regulator L5973. The failure is that the voltage on the output increases to 4-5V causing a damage in connected DSP chips. This is standard application from page 9 from the ST datasheet. Input is 12V output is 3,3V.

What can be a root cause of this behaviour? When I replace for new IC it is working in next coulpe of months ok and again fails.

Maybe somebody had this case and could share some ideas

Regards,

Pawel

This topic has been closed for replies.

2 replies

Visitor II
March 15, 2025

Hello, i am repairing a harman kardon with the same IC L5973scheme, i have one for 3,3V and another with 1,2V. The first step (3,3V) is damaged, measuring 4,9V.

I think the problem is age and moisture...

You only replace that IC or broken any more?

Thanks in advance

Senior III
March 15, 2025

L5973 has a max input voltage of 36V, so a strong spike can cause degradation over time.

Check with an oscilloscope if voltage spikes are exceeding 36V.

Use a TVS diode (like SM8S36A or SM8S33A) on the 12V input to clamp spikes.

Add a low-ESR bulk capacitor (1000µF, 25V or higher) to absorb transients.