Skip to main content
Cooke.Ernest
Associate III
January 4, 2018
Question

Keil Configuration Wizard - Doesn't Accept Decimal Point Numbers

  • January 4, 2018
  • 1 reply
  • 1070 views
Posted on January 04, 2018 at 18:11

Hi,

I have just started working on a configuration wizard utility in Keil uVision for the setup of stepper motors.

As can be seen, the configuration wizard so far setups the acceleration, deceleration, maximum and minimum speed etc. of the motor just fine.

However, for the distance per step option I would like to use a decimal point number, say 9.4 mm per step.  However the configuration wizard is not allowing me to enter decimal point numbers.

Is this a limitation of the configuration wizard or is there a method of entering decimal point numbers?

Any answers are greatly appreciated.

Thanks,

Ernest

0690X00000609MoQAI.png0690X00000609MeQAI.png

#powerstep01 #stm32f1 #configuration-wizard #dspin #stepper-motor
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
January 4, 2018
Posted on January 04, 2018 at 18:17

Might be better asked of Keil, and from a review of the documentation

http://www.keil.com/support/man/docs/uv4/uv4_ut_configwizard.htm

 

Suggest you use ASCII and then sscanf(), atof() or atod() the number, or use integers and scale.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..