Skip to main content
Efian.1
Associate II
May 26, 2020 9:37 AM UTC
Question

It appeared that nobody answer on spv1050 questions.. I had same problem as ask before : could not activate ldo if there are no charge ! even if battery is full! This is crazy! Also boost buck not working as expected.

Well, I have a lipoly single cell and ixolar solar cell from iXys (Vmpp = 4.3v) connect to the spv1050.

Buck boost not working correctly, efficiently is worst bad. (I got onlt a fraction of Amp from a direct connection to my battery!)

it is impossible to enable ldo without charge ( and vstore grow more than Veoc) !! this is crazy, so you could use your battery only if you have sun!?

I take time to verrify my design, test boost and busk boost configuration (shematic is same as demo board) I take time to calculate and recalculate all components from datasheet equations, I spent many many many time on it!

(I am electronic designer for more than 25 years)

So ST, where are you ?? nobody answer any questions on this chip ! This is crazy! no support nothing... so perhaps, electronics designer as me, was past behind something, or finally this chip is just a ***** ** ****! (unfortunately I select it in my last design, and this is a disaster!)

This topic has been closed for replies.

2 replies

Efian.1
Efian.1Author
Associate II
May 26, 2020 9:39 AM UTC

like I was censured I precise star replace : p i e c e o f s h i t !

YArbe.1
Visitor II
Jun 18, 2020 5:50 PM UTC

I have a similar issue here... No matter how much power is available in the sollar cell, the output from buck-boost converter cannot deliver more than 5 mA. It's very frustrating. If I put some load directly in the sollar cell in the same light conditions, I get over 30 mA. I reviewed my design many times, and can't figure out what could possibly be wrong.