Skip to main content
LKnuc.1
Visitor II
August 5, 2021
Question

Is VNQ660SP output STATUS pin Open drain ?

Hi, the datasheet of VNQ660SP do not specify if the STATUS pin is Open Drain or not. It is more clearly defined in other chip like the VN330SP.

In other word, we use many of the VNQ660SP on the same board and did connect the STATUS pin together. Is it ok ? Best regards, Laurent

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    July 13, 2023

    Welcome @LKnuc.1, to the community!

    The VNQ660SP has been obsolete for a very long time, so there is no official documentation for it anymore.

    If I remember correctly, one could also conclude from the data sheet that the STATUS pin was an open drain output, because only an output voltage low was specified. In this respect, it should have been possible to connect STATUS as a Wired-OR.

    If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.

    Good luck!
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.