Skip to main content
VICTOR1
Associate III
Feb 25, 2022 4:18 AM UTC
Solved

is this item have UL certificate for the STW4N150? our customer is request on UL on this component, is there anyone have the support documents? Thanks.

..

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Feb 25, 2022 9:18 AM UTC

    There are UL certificates only for safety-relevant features. Non-insulated transistors such as the STW4N150 have electrically accessible metal parts, which is why no UL certification is granted for them.

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    2 replies

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Feb 25, 2022 9:18 AM UTC

    There are UL certificates only for safety-relevant features. Non-insulated transistors such as the STW4N150 have electrically accessible metal parts, which is why no UL certification is granted for them.

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    VICTOR1
    VICTOR1Author
    Associate III
    Feb 25, 2022 9:39 AM UTC

    Got it, Thanks.