Visitor II
June 9, 2021
Question
Is there any sort of protection for "high" input voltages for the L7815CV?
- June 9, 2021
- 1 reply
- 1018 views
I am testing a L7815CV to charge a 12V Battery (I will use this in a solar system with a 20W solar panel where the input voltage might range from 0-22V and Imax=1.3A)
- When supplying an input voltage of 21V to the L7815CV, the L7815CV won't let any current pass.
- When I lower the voltage to below 16V, it starts to allow the current to flow.
- As I increase the input voltage, the L7815CV won't allow the current to flow anymore (in several trials, this voltage trigger where current stops to flow varies from around 17 to 20V)
- It will allow the current to flow again only if I lower the input voltage below 16V.
My questions:
- What is this behavior?
- Is this some sort of protection?
- could this be the internal limitation in power dissipation (Table 1. Absolute maximum ratings in the attached datasheet)? If so, what is this limit in Watts?
- What is the lifetime of such an L7815CV?
PS: temperature of the L7815CV was always below 60 Celsius during the tests.