Skip to main content
AHabe.1
Associate II
Jan 28, 2021 3:40 PM UTC
Solved

Is there a recommended methode to an insulated control of the ACST435-8?

..

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Feb 1, 2021 10:09 AM UTC

It always depends on your load - inductive/resistive/capacitive/mixture/etc.

You can find some information in e.g. AN4993, additional information can usually be found in the application notes from the suppliers of the (zero crossing) optocoupler.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

Peter BENSCH
ST Technical Moderator
Jan 29, 2021 12:34 PM UTC

Yes, by implementing galvanic isolation, e.g. using an optocoupler or zero crossing optocoupler, depending on your needs.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AHabe.1
AHabe.1Author
Associate II
Feb 1, 2021 9:07 AM UTC

Yes, of course we have to add an optocoupler or optotriac, but are there special requirements for the optocoupler or for the connection of optocoupler to the ACST435?

Is there an application note?

Thank you in advance.

Albert

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Feb 1, 2021 10:09 AM UTC

It always depends on your load - inductive/resistive/capacitive/mixture/etc.

You can find some information in e.g. AN4993, additional information can usually be found in the application notes from the suppliers of the (zero crossing) optocoupler.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AHabe.1
AHabe.1Author
Associate II
Feb 1, 2021 10:54 AM UTC

Thank you Peter.

The AN4993 is very helpful.

AHabe.1
AHabe.1Author
Associate II
Feb 17, 2021 7:45 AM UTC

Hi Peter,

now I have found the AN5114 on ST site.

This AN describes in a good manner the isolated controll of a TRIAC.

In chapter 3.3.1 there are the equations for determining the resistors.

But it seems that this equations do not really work for a ACST435 with 35mA gate current and for a photo-TRIAC with 1A surge current.

Could you please give me the recommended values for this TRIAC combination?

Thank you in advance

Albert

Peter BENSCH
ST Technical Moderator
Mar 4, 2021 8:52 AM UTC

The values for the surrounding devices depend on several factors of the environment. That's why ST also provides TRIAC, SCR and ACS Simulator to simulate is using your parameters, like e.g. load type, conduction mode, controller topology and heat sink.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.