Is the use of Reset and Alert Pins mandatory on STUSB4500BJR?
We are planning to use the STUSB4500BJR (WLCSP-25 package).
Since we want to avoid using micro-vias, we will not be able to fanout the inner 9 balls of the package.
This would afffect the following signals:
Pin B4 - CC1DB (not used, can be connected to ground)
Pin C4 - CC2DB (not used, can be connected to ground)
Pin D3 - ADDR0, connected to ground
Pin D2 - ADDR1, connected to ground
Pin C2 - A_B_Side, not used
Pin B2 - Alert
Pin D4 - Reset (would be hardwired to ground)
The above list only leaves the Reset and Alert pins unconnected.
Not connecting the Reset and Alert Pins would mean relying only on the I2C connection. So three question come to mind:
1. Is it safe to not use the RESET-Pin by directly connecting it to GND (with no pull-down resistor)?
2. Is it safe to not use the Alert Pin?
3. Is this a viable approach, or is there a circumstance where the RESET pin or the Alert-Pin is the only way to get the part working?
Thanks in advance,
Martin