Skip to main content
NBOUM.1
Associate
Feb 20, 2023 10:13 AM UTC
Solved

Is the STEVAL-CTM009V1 (L6491) capable to drive a stepper motor?

..

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Feb 20, 2023 12:51 PM UTC

Well, the STEVAL-CTM009V1 implements a three-phase driver with 5kW power, so it has three half-bridges, whereas a stepper motor typically requires two full bridges, i.e. four half-bridges.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Feb 20, 2023 12:51 PM UTC

Well, the STEVAL-CTM009V1 implements a three-phase driver with 5kW power, so it has three half-bridges, whereas a stepper motor typically requires two full bridges, i.e. four half-bridges.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.