Skip to main content
NPand.1
Visitor II
June 17, 2020
Question

Is it possible to use Viper12A with a bridge rectifier input instead of half wave rectification?

  • June 17, 2020
  • 2 replies
  • 670 views

I am using Viper12A as aux supply for sensors in a bigger Power supply system for sensors. I need to know if the line rectification circuit is possible using Bridge rectifier network. The output power needed is less than 1W with 16V output.

Thanks in advance.

This topic has been closed for replies.

2 replies

Peter BENSCH
ST Technical Moderator
June 17, 2020

You will find such a rectifier if you have a look at the datasheet of the VIPER12A, pg. 7.

So, yes, of course you can.

BTW: the VIPERs always "see" DC voltage coming from the capacitor behind the rectifier. It doesn't care if it is rectified using a single rectifier, a bridge rectifier or a 3 phase rectifier.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Peter BENSCH
ST Technical Moderator
June 17, 2020

.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.