Skip to main content
SSalm.1
Associate
Jan 23, 2023 9:50 PM UTC
Question

Is each MOSFET current limited to 1.7A in VNS1NV04DPTR-E? Or total current for the chip (both MOSFETs together) is limited to 1.7A?

..

    This topic has been closed for replies.

    3 replies

    Peter BENSCH
    ST Technical Moderator
    Jan 24, 2023 8:09 AM UTC

    In the data sheet of the VNS1NV04DP-E this is mentioned, but somewhat hidden on page 1 under the list of features as footnote 1:

    1. Per each device.

    Here each means each individual MOSFET and not both together.

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    SSalm.1
    SSalm.1Author
    Associate
    Jan 24, 2023 12:51 PM UTC

    Thank you for your response. That is what I thought too but wanted to check to make sure. Does this mean that in VNS3NV04DP-E the ILIMH 3.5A is shared between 2 MOSFETs since it does not have the "Per each device" note?

    Is RDS(ON) value the main difference between VNS1NV04DP-E and VNS3NV04DP-E?

    Peter BENSCH
    ST Technical Moderator
    Jan 24, 2023 7:31 PM UTC

    Well, that's actually a different topic for which a new thread should be created.

    However: VNS3NV04DP-E differs from VNS1NV04DP-E not only in the Rdson and thus the maximum current, but also in many other parameters (such as transconductance, switching times, input charge, or those of the drain source diode).

    It was also mentioned on page 1 of the VNS3NV04DP-E that the Rdson refers to each channel (i.e. one MOSFET), so I assume that this also applies to the current. If you want to be sure, you are welcome to confirm this question in the Online Support OLS.

    Good luck!

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.