Skip to main content
This topic has been closed for replies.

2 replies

RRach.2
Visitor II
Aug 23, 2022 9:28 PM UTC

Yep, from version 5.4.4+.

But it does not Generate with these versions, it wants 5.4.3 in order to Generate code, where the exmple is missing, but is built for that version.

The error in 5.4.4+ is:

ERROR [LineInfo_to_exitCode.manage_IocGenerationError] Unable to generate ioc file due to: When calling function "name", required parameter "gpio_port" (parameter #1) was specified, but had null/missing value....

Gigi
ST Employee
Sep 28, 2022 8:00 AM UTC

Tested right now

Using MC SDK 5.4.8

Opening the example, saving in a folder and generated using the update button

I'm using CubeMX 6.5.0 and Cube IDE 1.7.0

It compile with 0 error 0 warning. Not tested on real board just compilation.

Ciao

Gigi