Skip to main content
New.Fish
Associate III
September 17, 2024
Question

IPM for single phase motor control

There are several kinds of IPM, but it seems all 3 phase output.

Is there any IPM can do single phase motor control and how much is maximum output?

 

 

This topic has been closed for replies.

3 replies

Peter BENSCH
ST Technical Moderator
September 17, 2024

Three-phase control is considerably more powerful than single-phase control, and the demand is also considerably higher. With single-phase control, on the other hand, there are different motor types, so there cannot be a universal single-phase IPM. However, you could consider full bridges, e.g. PWD5F60 or PWD13F60.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
New.Fish
New.FishAuthor
Associate III
September 24, 2024

Thanks for your reply.

Both fully bridges are for small current (1A, 2A) load control, it can be for small motor control.

If I use STM32 MCU output pin directly connect to the PWD5F60 (or PWD13F60) input pin, should I use normal STM32 debugger for R&D development? because the IGBT output is high voltage which rectified from 240Vac. 

Peter BENSCH
ST Technical Moderator
September 24, 2024

What do you mean by IGBT, as both modules already contain a full bridge with MOSFETs?

The controlling STM32 is connected directly to the inputs of the devices, with the high side of the full bridge operating via internal level shifters. The base of the bridge is routed to GND either via a single shunt or two separate shunts so that the STM32 can measure the motor currents via the matching electronics and regulate them accordingly.

As the bridge is connected to the mains, you should use an insulating debugger like an ST-LINK/V2-ISOL or the B-STLINK-ISOL (adapter board for STLINK-V3SET).

Regards
/Peter
.

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.