Skip to main content
Associate III
September 11, 2026
Solved

Inherited legacy L99H01 / L99H02 design TS/ACT_OFF pin is N/C

I have inherited a legacy H bridge motor control hardware and firmware based on L99H01 (I think L99H02 might be drop in replacement). I’m a firmware developer - not a hardware designer, and I’m new to motor control, so I’m familiarizing myself with the hardware and firmware, and I’m having a “how can this have ever worked” moment.

The TS/ACT_OFF pin is not connected (floating). 

The value 0xC4 is written to REG3 by the firmware.

EXT_TS-bit = high (thermal sensor interface), and EXTTH[5:0] is set to 000100b (n=7, m=3) , giving

Vth = 7* (0.31 + 3*0.03) = 2.8V.

Vcc is 3.3V.

Apparently this design has functioned correctly for over 10 years, but since we will shortly be spinning a new board and porting the firmware to a new (ST) MCU I’d like to understand if there is a fundamental problem with this design.  All of the original hardware and firmware developers are long departed (probably retired 😑).

Thanks in advance if for any feedback.

 

 

 

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
September 11, 2026

Well, a floating TS/ACT_OFF pin is risky because its function depends on EXT_TS. With EXT_TS = 1, the pin is in thermal sensor mode; without a real diode chain, that is not the intended use. It may have “worked” thanks to leakage, noise margins, or accidental biasing of the floating node.

Recommendation: do not leave TS/ACT_OFF floating on the new board, but define it explicitly.

The value 0xC4 in REG3 is important because it sets RWD = 1 and EXT_TS = 1 and programmes EXTTH[5:0] = 000100b, which explicitly puts the device into thermosensor mode. However, without a proper diode chain, this is not usually the correct application.

If you are already doing a redesign, you should consider replacing this ancient L99H0x with something more modern, for example one with integrated MOSFETs?
What do you think about taking a look at the DC motor driver website or asking your local distributor?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
September 11, 2026

Well, a floating TS/ACT_OFF pin is risky because its function depends on EXT_TS. With EXT_TS = 1, the pin is in thermal sensor mode; without a real diode chain, that is not the intended use. It may have “worked” thanks to leakage, noise margins, or accidental biasing of the floating node.

Recommendation: do not leave TS/ACT_OFF floating on the new board, but define it explicitly.

The value 0xC4 in REG3 is important because it sets RWD = 1 and EXT_TS = 1 and programmes EXTTH[5:0] = 000100b, which explicitly puts the device into thermosensor mode. However, without a proper diode chain, this is not usually the correct application.

If you are already doing a redesign, you should consider replacing this ancient L99H0x with something more modern, for example one with integrated MOSFETs?
What do you think about taking a look at the DC motor driver website or asking your local distributor?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
sdtbbAuthor
Associate III
September 11, 2026

Peter, thanks for the quick reply. I agree that the next hardware spin should either include diodes, or tie TS/ACT_OFF to Vcc if it continues to be unused.

For the existing hardware would it be worth changing the REG3 configuration from 0xC4 to 0xFF, so that EXT_TS=1, but Vth evaluates to 0V ? Perhaps this would give the greatest margin against noise based triggering of the thermal sensor protection ?

I’m pretty certain that setting EXT_TS=0 is a non-starter, because there is no mention of an internal pullup on the TS/ACT_OFF pin, so I expect the motor driver would randomly cut out.

Visitor II
September 16, 2026

Hi sdtbb,
Your arithmetic holds. Tables 41 and 42 in DocID15567 map EXTTH 111 to n = 0 and m = 0, so 0xFF gives Vth = 0 V. Section 3.12.2 only trips when the pin sits below Vth for 64 µs, so nothing can trip it. On the part, ST lists all four L99H01 codes NRND today. The L99H02 (DS12547) keeps the same TS/ACT_OFF pin and REG3 bit layout, ST lists it active and Mouser shows 596 L99H02XPTR today.
Raz, Parter (AI supply chain app)