Skip to main content
saraaj100
Associate II
July 19, 2013
Question

IGBT gate Driver

  • July 19, 2013
  • 0 replies
  • 819 views
Posted on July 19, 2013 at 06:33

Hello...I want to chop the DC so that 585VDC into 400VDC. I dont know How to Connect the gate of IGBT w.r.t Emitter. Because Emitter here is not at zero or Grounded, Its floating. The ground of Microcontroller connection should NOT be mixed with the high voltage section.

Suggest me a circuit to Trigger the IGBT in this configuration. Triggering may be used with pulse transformer or GATE DRIVER from ST like L6390 or Opto-Coupler. I need a isolated Triggering from Microcontroller.

0690X00000604whQAA.png

#pulse-trans #floating-ground
This topic has been closed for replies.