IBUUI Board Updater fails to install IBUUI drivers for STEVAL-PCC009V2 board.
When I run the updater, and press 'start', an error occurs during the step, "Install IBUUI drivers". The error message is
Error installing C:\Program Files(x86)\STMicroelectronics\SPINFamily Evaluation Tool 3.2\Updater\Drivers\WinXP\IBUUI.inf driver. Access is denied
This file is present in the location and has read access by all groups listed under the file properties. I tried to run the IBUUI Board Updater as Administrator (right-clicking on it and choosing that option) but this did not change the behavior.
I also tried the alternate procedure to use STM32 ST-LINK software as described in the dm00268136 Spinfamily evaluation tool document, however once I try to connect to the MCU target, it says "No ST-Link detected."
Until this is corrected, I cannot use the eval6470PD board to continue my project.
The environment is Windows 10.