Skip to main content
NPrad.1
Associate
March 25, 2021
Question

i would like to kown whether you have support on Development board on BMS for E scooter

  • March 25, 2021
  • 3 replies
  • 748 views

Please follow the details:

we have 9P 17S battery setup

Battery Type : LiNiCoMnO2 (NMC) 

Nominal Voltage : 62.9

Upper Voltage: 71.4

Internal Resistance : ≤200mΩ 

Cell Voltage : 3.7

Please help us to select the hardware for our BMS. thank you

    This topic has been closed for replies.

    3 replies

    Peter BENSCH
    ST Technical Moderator
    March 25, 2021

    You could check our website Automotive Battery Management System (BMS), where you can find e.g. the BMS device L9963E and the corresponding SPI to isolated SPI transceiver L9963T.

    Please get in contact with your local distributor or the nearest local ST office to get more details and additional information.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    NPrad.1
    NPrad.1Author
    Associate
    March 25, 2021

    i have gone through few document, and it is mention that it will support cell up to 14 in series series. but we need 17 cell in series. do you have any development board for 17 cell in series. thank you.

    Peter BENSCH
    ST Technical Moderator
    March 25, 2021

    Yes, it is also mentioned at the first website mentioned above - in tab HW Evaluation Tools. You could use the EVAL-L9963-NDS, please don't be confused it is marked with NRND - it is an active part.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.