Suppose you are talking about the VN7140AS or VN7140AJ then its datasheet says:
Current limitation
The device is equipped with an output current limiter in order to protect the silicon as well as the other components of the system (e.g. bonding wires, wiring harness, connectors, loads, etc.) from excessive current flow. Consequently, in case of short circuit, overload or during load power-up, the output current is clamped to a safety level, IlimH, by operating the output power MOSFET in the active region.
The datasheet also mentiones IlimL with a typical value of 4A.
Please note: The limit values are also influenced by the chip temperature. Therefore, knowing your setup can be helpful in fully answering your question.
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.