Skip to main content
SkyWork
Associate III
Jan 18, 2021 8:25 AM UTC
Solved

I use single shunt algorithm to catch phase current, but check the 3 phase output side I can see there exist abnormal turn on/turn off signal as the attachment figure

..

This topic has been closed for replies.
SkyWork
SkyWorkBest answer
Associate III
Feb 6, 2021 2:37 PM UTC

I don't solve any issue, basic is is not a issue. the reason is that is ST's patent for catch current under one shunt architecture

ST will insert Zero vector (V0 or V7), in the special case for example when two of 3 phase duty cycle is to similar.

​

5 replies

Cristiana SCARAMEL
ST Employee
Jan 19, 2021 1:37 PM UTC

Hello @SkyWork​,

Which boards are you using?

Control method?

Application ratings?

For a better support, please share any other useful info.

"If you feel a post has answered your question, please click ""Accept as Solution"""
Cristiana SCARAMEL
ST Employee
Jan 22, 2021 10:03 AM UTC

Hello @SkyWork​,

do you still need Community support?

"If you feel a post has answered your question, please click ""Accept as Solution"""
SkyWork
SkyWorkAuthor
Associate III
Jan 27, 2021 12:54 AM UTC

Hello @Cristiana SCARAMEL​ 

I have clarified this issue thanks for your support

Cristiana SCARAMEL
ST Employee
Feb 4, 2021 3:02 PM UTC

Hello @SkyWork​,

could you share a summary about your issue and how you solve it.

In this way could help the Community members who might have similar concern.

"If you feel a post has answered your question, please click ""Accept as Solution"""
SkyWork
SkyWorkAuthorBest answer
Associate III
Feb 6, 2021 2:37 PM UTC

I don't solve any issue, basic is is not a issue. the reason is that is ST's patent for catch current under one shunt architecture

ST will insert Zero vector (V0 or V7), in the special case for example when two of 3 phase duty cycle is to similar.

​