Question
i need to charge 18650 li ion battery using SPV 1050 MPPT IC. where will i need to connect the load (microcontroller)? on which pin do i need to connect my micro controller?
Do i need to connect my load on STORE pin or in parallel to VBATT+ ?
In STEVAL-ISV020V1 what is EXT_SUP? is this where i need to connect my load
what will happen if i discharge 1 Amp current from 18650 battery?
what is the current capacity of inbuilt PASS TRANSISTOR?