Skip to main content
LHaac.1
Associate
October 20, 2021
Solved

I'm looking at the STEVAL-IHM023V3 board... What is the output voltage and amps?

  • October 20, 2021
  • 3 replies
  • 1044 views

..

This topic has been closed for replies.
Best answer by Peter BENSCH

The data are mainly to be found in UM1823: the voltage depends on input voltage and input configuration (voltage doubling or normal rectification) and the peak output current is discussed in point 2.3.5 (Overcurrent protection) and is 7A with the default settings.

Regards

/Peter

3 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
October 20, 2021

The data are mainly to be found in UM1823: the voltage depends on input voltage and input configuration (voltage doubling or normal rectification) and the peak output current is discussed in point 2.3.5 (Overcurrent protection) and is 7A with the default settings.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LHaac.1
LHaac.1Author
Associate
October 22, 2021

Hello Peter,

I see 7a is Shunt maximum but at what voltage...assuming input of 125vac would that be 7a and/or input voltage at 220vac would that still be 7a?

If I am able to set the output at 250v what would the amperage be?

Peter BENSCH
ST Technical Moderator
October 22, 2021

The default current limit is 7A - regardless of whether the input voltage is 125VAC, 285VAC or 400VDC.

Please also read the Terms and Conditions, which you can also find on the product website under the tab Documents, especially the RESTRICTIONS AND WARNINGS.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.