Skip to main content
JWang.38
Visitor II
February 4, 2023
Question

I am working on VND5T100AJ-E for HSD, wondering if any control option driver available from ST, or any one has control logic for overload, open-load in off-state actions?

..

This topic has been closed for replies.

1 reply

MBONA.1
ST Employee
October 25, 2023

The device is a simple switch with a diagnostic pin that gives us feedback on overload and open-load and general device condition.
There is no internal logic capable of triggering actions  in case of overload or open-load. except thermal protection. In case of thermal shutdown is triggered, the device can be programmed as auto-restart or latch-off, depending on FR_Stby status and according to "Table 11. Truth table".
All action have to be controlled either with a microcontroller or at application level, usually with external components.