Skip to main content
TShar.3
Visitor II
Jan 3, 2022 2:20 PM UTC
Solved

I am using STM32 based control board to control a pmsm. I am using a UCC27712 gate driver IC. Observing PWM pulses on scope, they seem to overlap and as duty ratio increases over lap increases. Is the "UCC27712 gate driver IC" is compatible with STM3

..

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jan 3, 2022 2:50 PM UTC

Welcome, @TShar.3​, to the community!

The question of compatibility is a bit confusing, as that can cover several aspects, such as level compatibility, but that doesn't seem to be a problem here.

As for the timing, the UCC27712 has an output interlock and 150-ns deadtime, so output overlap should not occur.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jan 3, 2022 2:50 PM UTC

Welcome, @TShar.3​, to the community!

The question of compatibility is a bit confusing, as that can cover several aspects, such as level compatibility, but that doesn't seem to be a problem here.

As for the timing, the UCC27712 has an output interlock and 150-ns deadtime, so output overlap should not occur.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.