Skip to main content
KN.1
Associate
January 8, 2020
Question

i am using L6566BH for high voltage SMPS. Its not turning ON with load. if its not connected with load then its working. Can you please check and revert with the solution.

  • January 8, 2020
  • 1 reply
  • 752 views

Input is 300 to 800V DC and output is 24V DC. Attached the schematics of the same.

This topic has been closed for replies.

1 reply

KN.1
KN.1Author
Associate
January 13, 2020

I could find solution by doing the experiments on this. Found the solution as the capacitor in Soft Start ( SS ) pin was not enough to reach the VCC to the required voltage level. Within this the IC is getting tripped. By increasing the capacitor in SS pin the problem has been addressed.

Regards

Kandababu N