Skip to main content
RGarc.646
Visitor II
October 30, 2019
Question

I am new to bldc motor control and recently purchased the EVAL6235Q evaluation board. Instead of buying the suggested communication board I am attempting to control by directly manipulating the input pins. Can this be done?

  • October 30, 2019
  • 2 replies
  • 873 views

Specifically I am pulling the 'motor direction' pin high, setting voltage reference pins accordingly and then setting the 'enable pin' high. The motor runs but I have no control to as the speed. Can this be accomplished or can this board only work with the suggested communication board? Does this communication board send a PWM signal to accomplish the different speeds? Any and all help will be greatly appreciated. Thank you.

This topic has been closed for replies.

2 replies

Thomas L.
Associate III
October 31, 2019

Well according to the datasheet the speed is set by setting VREF to some voltage. The datasheet also gives an example on how to build a control loop around VREF and TACHO but I haven't really worked with this part yet.

Cristiana SCARAMEL
ST Employee
October 31, 2019

​You can refer to AN1625 where you can find more details on the L6235 operation and how to implements an analog speed loop, a fine tuning of parameters is necessary (refer to page 25 and following).

A better solution is to implement an external digital loop (PLL or FLL) and use the integrated PWM current controller for the current loop limit.

"If you feel a post has answered your question, please click ""Accept as Solution"""