Skip to main content
GDavi.5
Visitor II
Apr 3, 2023 6:54 PM UTC
Question

I am looking to build a Power Supply that will vary between 2VDC and 15VDC in a Forward Converter Configuration. I need to produce an output of 200A.

I am looking to build a Power Supply that will vary between 2VDC and 15VDC in a Forward Converter Configuration. I need to produce an output of 200A. I have been advised by other engineers that I need to build a Parallel Configuration. I need a bit of technical support because I will be building variances from AC-DC Offline and DC-DC. I really do not know where to turn because the magnetics alone are a major obstacle. I know this can be done because there are commercial Power Supplies Available but are not completely compatible with what I need to do. Please connect me with a Field Applications Engineer that handles the Atlanta are.

This topic has been closed for replies.