Skip to main content
ALumb.1
Visitor II
Mar 27, 2023 11:35 AM UTC
Question

I am looking for a replacement of the Renesas driver HIP4086ABZ, 3-phase N-channel MOSFET drivers, specifically targeted for PWM motor control with a package size equal or lower. Thanks for your proposals

..

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    Mar 27, 2023 11:49 AM UTC

    Welcome, @ALumb.1​, to the community!

    You could either look at the STDRIVE101 with max 75V bus voltage, alternatively the STDRIVE601 for 600V.

    You can get more help from your local FAE or ST office.

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.