Skip to main content
HXu.11
Visitor II
Jan 10, 2023 9:37 PM UTC
Question

I am looking a solution to design protection for 12 to 16 cell battery pack. I think the L9963E or L9961 maybe work. It is a requirement that no MCU should be used. Can the IC be program with settings by external device and runs by itself without MCU

..

This topic has been closed for replies.

1 reply

KTANG.9
ST Employee
Jan 12, 2023 6:42 AM UTC

Hi,

L9961 supports up to 5x cells , max 25V. It can boot up and run diagnostics / voltage measurements without MCU at a basic level after initial programming of settings, but recovery from errors etc will require MCU intervention.

If 12 - 16 cell, it is advisable to use L9963E which supports up to 14 cells. Several devices can be stacked in a vertical arrangement in order to monitor up to 31 battery packs for a total of 434 series cells. MCU is needed.

You can download the datasheet here - https://www.st.com/resource/en/datasheet/l9963e.pdf

For ease of development, an evaluation board is available for purchase - https://www.st.com/resource/en/application_note/an5696-l9963e-evaluation-board-with-on-board-mcu-with-preloaded-firmware-gui-stmicroelectronics.pdf