HVLED805
Hello,
I want to execute my project with HVLED805 where input voltage is 176…264 V.
Output voltage for LED equal 18 V, output current 0.45 A.
Edesign proposed the transformer with widings: Primary – 145 turns, Aux – 29 turns, Secondary – 34 Turns, transformer core EE16, Reflected voltage 80 V.
I can’t allocate these winding therefore in program VIPer Design Software v.2.24 I have counted
analogous
transformer with widings: Primary – 120 turns, Aux – 17 turns, Secondary – 20 Turns, transformer core EE16, Reflected voltage 115 V.
Edesign recommended Rsense=0.931 ohm.
For calculation of this parameter with the new transformer I have used the equation (7) of datasheet (
Off–line LED driver with primary–sensing HVLED805 -
http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATASHEET/CD00287280.pdf
:(
Iout=(Npri/Nsec)(Vc_led/2Rsense)
In this equation
Iout
and
Vc_led
remains invariable.
After substitution of new values
Npri/Nsec
I have received Rsense=1.31 ohm
From here I had a first question: whether correctly I have made calculations?
In advance I thank you for the answer