Skip to main content
GoToHiro
Visitor II
June 23, 2021
Question

How to use STBB2

  • June 23, 2021
  • 0 replies
  • 481 views

Model: STBB2J30-R

The circuit is the same as "Figure 1. Application schematic for fixed version" on page 3 of the data sheet.

However, the output voltage is 2.8V instead of 3.3V.

Is there a similar event? If so, please tell me the details.

The settings are as follows.

VIN: 4.6V

EN: connected to VIN

BP: 0

MODE: 0

VSEL: connected to VIN

    This topic has been closed for replies.