Skip to main content
dungeonlords789
Associate III
Dec 29, 2020 9:38 PM UTC
Solved

How to select VCCVAL of powerstep01

I can select VCCVAL to 7.5 V or 15 V. In which case I need 7.5 V? In which case I need 15 V?

This topic has been closed for replies.
Dario CUCCHI
Dario CUCCHIBest answer
ST Employee
Jan 11, 2021 9:51 AM UTC

7.5V can be useful if the voltage supply VS is less than 18V and your application need a regulated voltage for the gate drivers.

In this case the linear regulator cannot provide 15V (because its input is too low)

Power MOSFET are driven using the VCC, so higher is the voltage lower the Rds,on.

Switching loss due to the gate charge are higher with 15V (however we are talking about few mA).

My suggestion is to use VCCVAL = 15V if the Vs in your system is greater than 18V.

1 reply

Dario CUCCHI
Dario CUCCHIBest answer
ST Employee
Jan 11, 2021 9:51 AM UTC

7.5V can be useful if the voltage supply VS is less than 18V and your application need a regulated voltage for the gate drivers.

In this case the linear regulator cannot provide 15V (because its input is too low)

Power MOSFET are driven using the VCC, so higher is the voltage lower the Rds,on.

Switching loss due to the gate charge are higher with 15V (however we are talking about few mA).

My suggestion is to use VCCVAL = 15V if the Vs in your system is greater than 18V.