How to reconfigure STEVAL-ESC001V1 to hall inputs
The gui allows reconfiguring to HALL inputs, which is why we purchased these boards. To test some motors during fast startup using hall sensors.
When setting up HALL inputs there appears to be no valid pin configuration to get the sensors connected. Default is to use the current sense inputs A0, A1 and A2 but this is driven by U3, U4 and U5 on the board.
Depending on which timer is used I find multiple alternatives for pins, most relate to a larger chip than is used on the STEVAL-ESC001V1 board.
I did identify following "free" pins:
TP3 PB4
TP4 PC13
TP8 PA4
TP9 PA5
INPUT PA15
TP2 PB8 CAN_RX
TP1 PB9 CAN_TX
But, with TIM3, only the first two channels can be set up.
But third channel needs one of E4, B0, C8 none of which appear available.