Skip to main content
Aurélien f
Associate III
November 10, 2017
Question

How to protect the 3.3V stm32 line ?

  • November 10, 2017
  • 0 replies
  • 500 views
Posted on November 10, 2017 at 13:52

Hello, 

I'm facing an issue regarding the 3.3V line on my board that embeds a stm32. The board also embeds a radio module (WISOL SFM10R1). My problem is that at one moment my radio module seems to be blown because it no longer responds but the stm32 is still working well. So i'm suspecting my supply board that is generating the 3.3V to overshoot this voltage. This board embeds a bq25570 from TI (

http://www.ti.com/lit/ds/symlink/bq25570.pdf

 ).

So, to prevent this over voltage i intend to put a 3.3V TVS diode between the supply board and the main board (stm32 + sfm10R1) such as :

https://www.mouser.fr/ProductDetail/Comchip-Technology/CPDH3V3UP-HF/?qs=sGAEpiMZZMsItbzKdwyIe6GoLhY6dGANVOZha8o4%2fPY%3d

 

The idea is to stay in ultra low power, so the protection circuit needs to have a very low current consumption.

So, i would like to know if this solution can work, or if there is a better solution.

Best regards,

Aur�lien

#stm32 #transil #tvs #3.3 #protection
This topic has been closed for replies.