Skip to main content
BL1
Associate III
Nov 23, 2021 9:29 AM UTC
Solved

How to configure POWERSTEP01 ocd_th in current mode?

Hi,

Using IHM03A1, I try to drive a 48V-9A motor.

I've set up the POWERSTEP01 driver in current mode, with default registers values, which works nicely but with low torque. Now I want to increase current up to 9A.

I've changed IHM03A1 R1 and R2 resistances to 15mOhm+-1% / 3W ones.

According to current mode , I've set ALARM_EN to 0x8F ( disable ADC UVLO, disable stall detection, disable switch).

Last thing to do is to increase OCD_TH to enable 9A . But OCD_TH is set in Volt, which resistance value should I use for the convertion.

Thanks

This topic has been closed for replies.
Cristiana SCARAMEL
ST Employee
Nov 30, 2021 12:42 PM UTC

Hello @BL​,

the powerSTEP01 measures the load current of each phase sensing the VDS voltage of the all integrated MOSFETs.

You can estimate the drop on the MOS using the Rdson typical value at 125 °C (23 mohm).

For the high side MOSFETs --> Vocd = 23 mOhm x 9 A = 207 mV

For the low side you have to calculate the threshold taking into account also the drop on the sense resistor.

Vocd = (23 + 13 ) mOhm x 9 A = 324 mV

In general, when you set the OCD threshold you should taking into account of the Rdson variation in temperature.

Moreover lower threshold is more sensitive to a noise.

"If you feel a post has answered your question, please click ""Accept as Solution"""

3 replies

Cristiana SCARAMEL
ST Employee
Nov 30, 2021 12:42 PM UTC

Hello @BL​,

the powerSTEP01 measures the load current of each phase sensing the VDS voltage of the all integrated MOSFETs.

You can estimate the drop on the MOS using the Rdson typical value at 125 °C (23 mohm).

For the high side MOSFETs --> Vocd = 23 mOhm x 9 A = 207 mV

For the low side you have to calculate the threshold taking into account also the drop on the sense resistor.

Vocd = (23 + 13 ) mOhm x 9 A = 324 mV

In general, when you set the OCD threshold you should taking into account of the Rdson variation in temperature.

Moreover lower threshold is more sensitive to a noise.

"If you feel a post has answered your question, please click ""Accept as Solution"""
BL1
BL1Author
Associate III
Nov 30, 2021 2:37 PM UTC

Hello @Cristiana SCARAMEL​ ,

Thanks

As I don't want to be noise sensitive, so if I well understood, I should set OCD_TH to 324mV.

But as I don't want overcurrent detection to trigger for notiong, do you recommand to set it a little higher? With OCD_TH = 324mV , every time current will be a little higher 9A, overcurrent flag will trigger, or is there already a tolerance?

Cristiana SCARAMEL
ST Employee
Dec 1, 2021 2:20 PM UTC

Hello @BL​,

in your case you can round up to the typical value 343.75 mV (OCD_TH = '1010').

As reported in the datasheet (Table 4 pg 15), the OCD voltage threshold is equal at typical value ±10%

"If you feel a post has answered your question, please click ""Accept as Solution"""