Skip to main content
MPico.2
Associate
Mar 22, 2023 10:40 AM UTC
Question

How to configure in NVM STUSB4500 PDOs without reverting to its previous configuration when powered off ?

I'm using the Software library "STSW-STUSB003" to configure STUSB4500 PDOs,

I use the STEVAL-ISC005V1 with the stm32F072RB. my program works, I manage to modify the PDOs to get the desired voltage.

But when the evaluation kit is disconnected, it reverts to previous configuration. So I can't configure the PDO permanently except using the "STSW-STUSB002" GUI

I only use I2c signals between the stm32 and the eval kit.

I'm using this function from "USB_PD_core.h" to set PDOs

 Update_Valid_PDO_Number( Usb_Port, 3 );

 Update_PDO(Usb_Port, 1, PDO_V1, PDO_I1); 

 Update_PDO(Usb_Port, 2, PDO_V2, PDO_I2); 

 Update_PDO(Usb_Port, 3, PDO_V3,PDO_ I3);

    This topic has been closed for replies.

    2 replies

    ST Employee
    Mar 22, 2023 10:57 AM UTC

    Hello,

    STSW-STUSB003 is a software library to be used for dynamic power profile modification, and it is not saving permanently the configuration indeed.

    But from st.com, you can also download a utility called STSW-STUSB004, to be used to translate the configuration defined with STSW-STUSB002 GUI into the Non Volatile Memory of the IC. This will make the change effective at every Power On Reset.

    Rgds,

    Benoit

    MPico.2
    MPico.2Author
    Associate
    Mar 22, 2023 11:07 AM UTC

    Ok Thank you for your reply !