Skip to main content
VAkul.1
Associate II
August 23, 2021
Question

Hi, We are using LED driver (LED2472GBTR) in one of our products. Can we make RGB[1:8] outputs high (VDD=3.3V)? If so how? Regards, Veera

  • August 23, 2021
  • 9 replies
  • 1727 views

..

This topic has been closed for replies.

9 replies

Peter BENSCH
ST Technical Moderator
August 25, 2021

Welcome, @VAkul.1​, to the community!

Actually, you only need to switch / OE inactive to have all outputs also inactive. However, the outputs are not push-pull stages, but current sinks, the current of which can be set with a resistor connected to iset.

Are you aware that VDD is not limited to 3.3V, but can be between 3...5V?

What do you want to achieve by setting all outputs high?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
VAkul.1
VAkul.1Author
Associate II
August 25, 2021

Hi Peter,

Thank you for the Reply.

Actually we don't want to inactive all outputs. We want to control R[1:8], G[1:8] and B[1:8] outputs independently.

Can we control these Outputs independently low or high (particular segment LED on/off). If so how?

Regards,

Veera

Peter BENSCH
ST Technical Moderator
August 25, 2021

Hi, Veera,

Of course, you can set all outputs independently of each other as you like. However, the LED2472G is controlled serially (works as a serial-parallel converter) and therefore the data of all 24 outputs have to be rewritten for every change of only one output, even if their level is unchanged.

Regards

/Peter

BTW: please don't use your email to answer, as it contains your phone number, which is visible worldwide for every reader of the community.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.