Skip to main content
_Sansindhu
Associate
Sep 12, 2022 1:36 PM UTC
Question

Hi I would like to use external MOSFET with ST's eFuse part STEF01, because of my Bus Voltage is 145V and bus current would be 3Amp. Pls suggest possible solution. Thanks.

..

    This topic has been closed for replies.

    3 replies

    Peter BENSCH
    ST Technical Moderator
    Sep 12, 2022 1:48 PM UTC

    Welcome, @_Sansindhu​, to the community!

    STEF01 can drive an external FET, but it is in series and only serves to protect against polarity reversal. Since the STEF01 is connected to the full input voltage, but is destroyed above 55V, it cannot work with your 145V.

    By the way, all our e-fuses currently work up to a maximum of 55V, so we cannot yet recommend a possible solution.

    Does it answer your question?

    Regards,

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    _Sansindhu
    Associate
    Sep 16, 2022 5:28 AM UTC

    Thanks Peter!

    Peter BENSCH
    ST Technical Moderator
    Sep 19, 2022 7:49 AM UTC

    Your're welcome!

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.