Skip to main content
ezuk
Visitor II
December 17, 2018
Question

Hi, I'm looking for the solution that can take 5V solar panel input and charge 4.2V lithium battery.

  • December 17, 2018
  • 0 replies
  • 389 views

Hi,

I'm looking for the solution that can take 5V solar panel input and charge 4.2V lithium battery. I also need to be able to provide the power to the rest of the system even when the battery is not connected. I was looking at SPV1050 IC but I'm not sure if I can use it with a load. Any suggestions?

Thanks!

Emilija

This topic has been closed for replies.