Skip to main content
FVill.5
Visitor II
Jul 13, 2022 12:39 AM UTC
Question

Hi, I am currently working with the STGAP1AS gate driver. I have an issue with the program not working after the driver loses power. Is there any way to preserve the program when the power is lost for the STGAP1AS or the STGAP1BS gate drivers?

..

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    Jul 13, 2022 10:40 AM UTC

    Welcome, @FVill.5​, to the community!

    Well, if the power supply to the gate driver fails, the subsequent power stage is also affected. So you should monitor the power supply of both the gate driver and the power stage and reinitialise the gate driver as soon as the power supply is restored.

    Does it answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.