Skip to main content
aadza.1
Visitor II
Jun 21, 2022 3:34 AM UTC
Question

Hi, Could you give some information regarding this component, Part No : LD1117S50TR Can you give information regarding pin dimension marked with X (refer image) Thank you

..

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    Jun 21, 2022 8:44 AM UTC

    Welcome, @aadza.1​, to the community!

    We would like to apologize that this information was not taken over from the standard JEDEC TO-261: the value X and Y in your drawing is called L by JEDEC and the value min 0.75mm is given, typical and max values do not exist for this value.

    Does it answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.