Skip to main content
Visitor II
Nov 4, 2026 3:19 PM UTC
Question

Help Designing Power System

Hello, I am designing the power supply section for my board.

The connector on the left is intended to connect to a LiPo battery. My voltage regulators and the BQ2407 are arranged in a pyramid-like configuration: there are three LDOs beneath the BQ2407, and below those, two buck converters. I’m reaching out because the current layout doesn't look very aesthetic, and I’m struggling to find a way to make it appear more professional.

Any advice would be greatly appreciated. Thanks!

 

2 replies

Peter BENSCH
ST Technical Moderator
Nov 9, 2026 7:43 AM UTC

Welcome ​@yisusyisusyisus, to the community!

It is understandable that you place importance on the appearance of your board. However, with electronic devices, functionality, reliability, and compliance with applicable regulations are generally decisive.

So that you can be helped here in the ST Forum in a targeted way, it would also be helpful to understand what relation your project has to ST devices. That is not yet clear from your post.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Bruce Jones Harry
Associate
Nov 9, 2026 8:38 AM UTC

Hi ​@yisusyisusyisus 

Looks matter less than function here, so I’d focus on a few basics: keep each buck converter’s input loop (input cap, IC, GND) and switch node as small as possible, with the input cap right at the VIN/GND pins. Use a solid ground plane underneath, and keep the LDOs and any sensitive circuitry away from the switching section. Also follow the BQ2407 datasheet’s layout guidelines. A neat layout comes naturally when parts are aligned, evenly spaced, and well labeled on the silkscreen.

As ​@Peter BENSCH  said, it would help if you could share your schematic and which ST device is involved.

Regards
Bruce Jones Harry