Skip to main content
KRönn.1
Visitor II
June 16, 2020
Question

Hello, Is it Ok to use VNH5180A-E Vcc power value 30V (Abs max is 41V and Op supply voltage max is 18V) ?

  • June 16, 2020
  • 1 reply
  • 555 views

VNH5180A-E

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
June 16, 2020

The VNH5180A-E is an automotive device, so it must withstand/survive test pulses at the supply line, which are defined in ISO 7637-2:2004(E), see the datasheet, pg 16. There is a built-in overvoltage clamp to fulfil these requirements.

So, it is not OK to run the VNH5180A-E permantely with 30V. The recommended operating conditions can be found in the datasheet pg. 9 under Electrical characteristics, giving for Vcc=5.5...18V.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.